{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you set up the ATV320 drive so that the digital DO output controls output contactor command OCC?
Issue:
Set up the ATV320 drive so that the digital DO output controls output contactor command OCC.

Product Line:
ATV320

Environment:
All

Cause:
Wants to set up the DQ or DO so that it controls the a output for OCC.

Resolution:

Wiring:
Jumper +24vdc to DQ+
Wire your + side of your relay coil to DQ-
Wire the other side of the coil to Com

Programming:
In the Application Function Menu, set OCC to DO1

Schneider Electric Egypt and North East Africa