Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How do I manage to calculate the actual relay trip time for phase overcurrent protection (ANSI 50-51) of self powered protection relay VIP 45?
The overall protection graph for Phase Overcurrent Protection (ANSI 50-51) is presented by multiple segments as follows:
Calculation of tripping time in terms of settings for each curve/segment can be summarized as detailed in attached file.
Calculation of tripping time in terms of settings for each curve/segment can be summarized as detailed in attached file.
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: