Issue
How to find out what measurements Powerlogic and/or ION meters should be logging by default
Product Line
Power Monitoring Expert 7.2.2
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024
Environment
PM200
PM800
PM5000
ION6200
ION9200
ION9300
ION7300
ION7500
ION7600
ION7700
ION8300
ION8600
PM8000
ION9000
micrologic trip units
Cause
Not all meters use the same templates or have the same default measurement maps for onboard logging
Some meters do not have the capability of onboard logging
Resolution
- Please find the attached excel document to identify the default logged measurements sorted by device type
- Set "Logged by Default" to Yes
- Select the device type you wish to inquire
- Use the "Row Label" section to view the default measurements
NOTE * If the "Row Labels" portion of the document is blank when "Logged by Default" is set you yes, then the meter does not have onboard logging capabilities and software logging must be configured
Please use article: How to setup PC based logging in the ION Enterprise VIP when a device does not have onboard logging capability. | Schneider Electric USA to help.