{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Wire recommendation to use with EM4200 series meters
Issue
Wire recommendation to use with EM4200 series meters

Product Line
EM4200 series meters
EM4235
EM4236

Environment
Meter wiring

Resolution
The EM4200's recommended wire size for I/O, Communications, and CT is 24-16 AWG (0.2 to 1.5 mm2) shielded wire, solid or stranded.

Schneider Electric Egypt and North East Africa