Issue:
ATV320 to use the dial of drive as speed reference and Digital Input 1 (DI1) terminal as start/stop control
Product Line:
Altivar 320, ATV320
Environment:
All
Cause:
Programming setup
Resolution:
From Main Menu, press enter.
Scroll down to CONF and press enter.
Scroll down to FULL and press enter.
Scroll down to CTL and press enter.
Under CTL, set CHCF to SEP.
Set FR1 to A1U1.
Set CD1 to TER.
From the normal status display, press enter twice to then adjust the speed reference value as a % of the LSP-HSP range.
ATV320 to use the dial of drive as speed reference and Digital Input 1 (DI1) terminal as start/stop control
Product Line:
Altivar 320, ATV320
Environment:
All
Cause:
Programming setup
Resolution:
From Main Menu, press enter.
Scroll down to CONF and press enter.
Scroll down to FULL and press enter.
Scroll down to CTL and press enter.
Under CTL, set CHCF to SEP.
Set FR1 to A1U1.
Set CD1 to TER.
From the normal status display, press enter twice to then adjust the speed reference value as a % of the LSP-HSP range.
Released for: Schneider Electric Egypt and North East Africa