{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I setup Level Control on an Altivar 600 Process Drive?

Issue:
How do I setup Level Control on an Altivar 600 Process Drive?

Product Line:
Altivar 600 Process Drive (ATV630, ATV650, ATV660, ATV680)

Environment:
All serial numbers for Altivar 600 Process Drive

Cause:
N/A

Resolution:
Level Control
In many water and waste water applications, centrifugal pumps and submersible pumps are used for emptying or filling tanks/towers
The objective of this function is to avoid level overflow in tanks during the filling process and the complete emptying of tanks at the emptying process.
​-  Function should fill or empty a tank according to the request by:
-  Control the speed of 1 Variable Speed Pumps (VSP)
-  Staging / De-staging x Fixed Speed Pumps (FSP) with (x = 5 for ATV6xx)
or Variable Speed Pumps (VSP)

Multi-Drive Link
-  Firmware V1.6 + option card VW3A3721 (Multi-VFD Ethernet Comms Module for ATV6xx)
-  Used for Multi-Drive in Multi-Pumps mode
-  Must use standard Ethernet cables with communication network configured with fixed IP addresses

Procedures
-  For step by step procedures reference attached document.

NOTE:
- Function is not available on the Altivar 900 series drives (ONLY Altivar 600)
- For Multi-Drive configurations you need Multi-Drive Communication Card (VW3A3721)


If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Egypt and North East Africa

Attachment(s)
ATV6xx_Levelcontrol.pdf [513.08 KB]