{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the specification on the ATV320 Internal +24Vdc power supply?

Article available in these languages: Spanish

Issue:
ATV320 internal +24Vdc power supply specifications.

Product Line:
Drives

Environment::
All

Cause:
Installation / Setup

Resolution:

+24 Vdc, sampling time 2 ms, maximum voltage 30 V, maximum current 100 mA  this supply is used for turning on the logic inputs.

Also note that the P24 is not a input for external supply.   The P24 is a output supply for the STO safe torque off input.

Schneider Electric Egypt and North East Africa

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: