Search FAQs
Can the ATV212 or the ATV320 Drive accept multiple motor wires directly on its terminals or external terminals are required?
Issue:
Does ATV212 or the ATV320 Drives accept multiple motor wires directly on its terminals or external terminals are required?
Product Line:
ATV320, ATV212
Environment:
All
Cause:
NA
Resolution:
It is not recommended to connect 2 motor wires to 1 drive's output terminal for ATV212 and ATV320. Need to do it externally.
Does ATV212 or the ATV320 Drives accept multiple motor wires directly on its terminals or external terminals are required?
Product Line:
ATV320, ATV212
Environment:
All
Cause:
NA
Resolution:
It is not recommended to connect 2 motor wires to 1 drive's output terminal for ATV212 and ATV320. Need to do it externally.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: