{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the ATV630 be powered up with only the 24VDC control voltage to set the parameters?
Issue:
Can the ATV630 be powered up with only control voltage?

Product Line:
ATV630

Cause:
n/a

Resolution:
Yes.  The ATV600 Series is rated to bring external +24VDC supply and wire to P24 and bring external common to 0v to power up the display and can change the parameters.

Schneider Electric Egypt and North East Africa