Search FAQs
Com'X 210/510 GPRS SIM card Overview
Issue
Com'X 210/510 GPRS Settings
Product Line
Com'X 210
Com'X 510
Environment
Installation/Setup
Cause
GPRS access settings depend on the GPRS modem that is connected.
Resolution
The SIM card is embedded in the GPRS modem. You can only use the EBXA GPRS SIM to publish data if you are exporting data to Remote Service Platform. The settings of this GPRS access are set by the Com'X.
The reference EBXA-GRPS-SIM must be selected for the GPRS modem.
This graphic shows the interface for accessing the GPRS modem with an EBXA GPRS SIM card:
Figure 1: Com'X Webpage
NOTE:
For the Com'X that comes with the SIM card included: The SIM card that comes with the Com'X 510 is Vodafone, but will connect to the T-Mobile network in the United States once the card is activated.
For the Com'X without the SIM card included: Provided that the cellular provider will allow the equipment on their network, and the user configures the proper APN and SIM card settings, there are no constraints for putting the ComX on another GPRS network.
Com'X 210/510 GPRS Settings
Product Line
Com'X 210
Com'X 510
Environment
Installation/Setup
Cause
GPRS access settings depend on the GPRS modem that is connected.
Resolution
There are 2 reference numbers for the GPRS modem:
- EBXA-GPRS-SIM
- EBXA-GPRS
The SIM card is embedded in the GPRS modem. You can only use the EBXA GPRS SIM to publish data if you are exporting data to Remote Service Platform. The settings of this GPRS access are set by the Com'X.
The reference EBXA-GRPS-SIM must be selected for the GPRS modem.
This graphic shows the interface for accessing the GPRS modem with an EBXA GPRS SIM card:
Figure 1: Com'X Webpage
NOTE:
For the Com'X that comes with the SIM card included: The SIM card that comes with the Com'X 510 is Vodafone, but will connect to the T-Mobile network in the United States once the card is activated.
For the Com'X without the SIM card included: Provided that the cellular provider will allow the equipment on their network, and the user configures the proper APN and SIM card settings, there are no constraints for putting the ComX on another GPRS network.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: