Search FAQs
How ClearSCADA can access an SQL database across the network from a remote computer that does not have ClearSCADA’s ODBC driver installed?
Issue
Access and control an SQL database exists on a remote computer that does not have ClearSCADA's ODBC driver installed on it.
Product Line
ClearSCADA 2015R2
Environment
Microsoft Windows Operating System, ClearSCADA 2015R2 ViewX, SQL
Resolution
This resolution discusses how ClearSCADA can access and control SQL Database using the ODBC driver.
Step (1): Data Source Name "DSN" Configuration
When it is required to establish a connection between a ClearSCADA system and a Third Party ODBC Client, a name for the data source to be defined.
To define the Data Source Name (DSN), display the ODBC Setup window, then enter the required DSN in the Name field as shown in the below steps.
- Open Data Sources (ODBC) from the control Panel
- Click on the Second Tab System DSN
- Click on Add
- Select the SQL Server Driver from the scroll down menu
- Click on Finish
- Type a name for the DSN, for example SQLDB
- Type the remote computer name followed by the SQL server name that exists on the remote computer, or select it from the drop down list (it might take few moments to search for the available SQL servers)
- Click on Next
- Select the Authenticity that will allow ClearSCADA to log in to the SQL server.
- In this example the existing user on SQL is utilized Login ID: sa
- Click on Next
- On the remote computer open Microsoft SQL Management Studio
- Right Click on the server list and select Properties
- Click on Security
- Select SQL Server and Windows Authentication Mode
- After logging on to the SQL server, select which database will shall be controlled
- Activate the Check Box "Change the default Database to:"
- Select the SQL database name from the menu, for example call the database CS on SQL
- Click on Next
- Click on Finish
- Click on Test Data Source to confirm the connection is successfully established
- Finally the DSN is configured and ready to be linked to the ODBC connection on ClearSCADA
Step (2A): ClearSCADA, ViewX configuration to read data from the SQL database
- Open ViewX
- Create a new Group on ViewX for example "ODBC_Example"
Creation of a new ODBC Connection
- Right Click on the new group "ODBC_Example", Create New > ODBC > Connection
- Open the new connection properties window
- Type name of the DSN, or select the DSN that was configured in Step-1 from the menu
- Type User name "sa", and Password of the SQL Server User
- To confirm the new ODBC connection is working properly, check its state by right clicking on the New Connection and select "View Status" that should be showing "Online"
Creation of a new ODBC Query
- Right Click on the new group ODBC_Example > Create New > ODBC > Query
- Type the ODBC connection name "New Connection", or select it from the menu
- Write a query for example a query to read all data exists in the SQL database "SELECT * FROM CSDB"
Creation of a new Analog Input Point
To show a value from the SQL database on a ClearSCADA mimic
- Right Click on the new group ODBC_Example > Create New > ODBC >Analog Point
- Open the New Analog Point properties
- Type the query name "New Query", or select it from the menu
- Select one of two options to poll data from the SQL database either Row & Column, or Value Lookup
Reading Analog values from the SQL database
- Assume that Row & Column method shall be defined to read data from the SQL database
- Select "Row & Column" from the "Lookup Method"
- Type "3" in Row cell, and "2" in Column cell
- Show the Analog Input point on the mimic to see its value online
- Snapshot from the SQL server, shows value of cell (3,2)
Step (2B): ClearSCADA, ViewX configuration to write data on the SQL database
Modifying the SQL database
Using a query that would modify the value of the same cell (3,2), which is being read in the previous Step-2A
- The query can be written like "UPDATE CSDB SET Age=85 WHERE ID=3;"
- Mimic screenshot:
- SQL Server Screenshot:
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: