{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ATV212- customer wants to monitor the fan so it will set an alarm in their Modbus register to let them know the fan is not running, before the drive faults
Issue:
Set Alarm for Modbus Register.

Product Line:
ATV212

Environment:
Modbus

Cause:
n/a

Resolution:
There is a Flashing L in the drive. This is to let you know you are getting close to a overheating fault. You can monitor this parameter ( FC91- register 64,657, bit 3 is the motor overload alarm).

Schneider Electric Egypt and North East Africa