{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I synchronize the M580 PLC clock by BMENOC03X1 NTP service ?

Issue:
Can I synchronize the M580 PLC clock by BMENOC0301/11 NTP service ?

Product Line:
M580

Environment:
EcoStruxure Control Expert

Resolution:
In order for the time on the CPU module to synchronize with the BMENOC NTP service, you need to enable the network time service, in the DTM browser of the BMENOC, ,then select the checkbox  "Update CPU time with this module".
The project will need to be built and downloaded to the CPU.

Schneider Electric Egypt and North East Africa