{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How are the basic parameters set up in ATV320 Drive?

Article available in these languages: Czech, Spanish, Finnish, Korean

Issue:
Parameters to set up in a ATV320 Drive.

Product Line:
Altivar 320

Environment:
All ATV320 drives

Cause:​
Basic programming

Resolution:
CONF>FULL>SIM
tFr= Max frequency
ItH= Motor thermal Current (motor FLA)
ACC= ramp up time
dEC= ramp down time
LSP= Low speed
HSP= High speed

CONF>FULL>drC
bFr= Base motor frequency 60hz

CONF>FULL>drC>ASY
nPr= HP of the motor
UnS= Rated motor voltage
nCr= Rated motor current (Motor FLA)
FrS= Rated motor frequency
nSP= Rated motor speed (RPM)

CONF>FULL>SET
CLI= current limit (maximum current, must be greater than FLA, up to 150% of FLA)

NOTE: Make sure to use the information on your motor's nameplate for programming. 

Please refer to ATV320 Programming Manual, document # NVE41295 for additional details.

 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
move-arrow-top