{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the CFI2 fault on an Altivar (ATV600, ATV900 and ATV340) drive?

Article available in these languages: Turkish

Issue:
Customer has the CFI2 fault on an Altivar Process Drive

Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980, and APM)
Altivar Machine Drive (ATV340)

Environment:
All serial numbers

Cause:
N/A

Resolution:
The CFI2 is Configuration Transfer Error Fault.
Occurs when a configuration file can not be loaded to the device, or the configuration is not compatible with the drive.

Possible Causes:
  • The was an unsuccessful or interrupted configuration file transfer.
  • The stored configuration (HMI) was loaded from an different firmware.  For example a file saved on a newer version drive can not be loaded into an older firmware version.
Remedies:
  • Check firmware
    • Firmware should be compatible on both drives
  • Load a compatible configuration.
  • Use SoMove to transfer configuration from another drive, or modify the saved SoMove configuration to match the drive being programmed.
  • Perform a factory setting
    • [Main Menu] [File Transfer] [Factory Settings]

Schneider Electric Egypt and North East Africa