{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Power Monitoring Expert 8.2 - When I run Report Generator (RepGen) from either an Engineering or Reporting Client, choosing 'Manage' causes a run-time error
Symptoms:
I launch Report Generator (the Excel-based reporting tool) on either an Engineering Client or a Reporting Client.
I choose the 'Manage Reports' radio button, and select any report.
At this point, an error dialog appears with the following text:

Run-time error 91:
Oject variable or With block variable not set


Workaound:
This will only happen if RepGen is run from either and Engineering or Reporting client and the version of Excel used is a newly installed x86 (32 bit) version of Excel 2013. The 64-bit version will work fine, as will the 32-bit versions of Excel 2007 and Excel 2016, as will using any  version of Excel and running RepGen on the server.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.