{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
For SSR relay, which EMC-relevant parts of the EN 61000 standard are met, in particular, is it part 1 + 3?
NO, there is no EMC declaration on our EU DOC certificate. See attached file, EU DOC - 2016  SSP3 SSM1 SSM2 SSL1 SSLZ.pdf.

Here is the reason, refer to IEC62314:2006 standard.

Solid state relays are components (not stand alone devices) and as such do not perform a
direct function. Therefore, no EMC requirements are included in this standard.

NOTE This is in line with the European EMC Directive.

Schneider Electric Egypt and North East Africa

Attachment(s)
EU DOC - 2016 SSP3 SSM1 SSM2 SSL1 SSLZ.pdf [212.02 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.