{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to change the template on an ATV630 and ATV930 so that the 0% speed is at low speed, instead of 0 hz?

Article available in these languages: Spanish

Issue:
Wants to change the template on an ATV630 and ATV930 so that they show 0 % speed is at low speed, instead of 0 hz

Product Line:
ATV630 ATV930

Environment:
Pedestal and deadband

Cause:
n/a

Resolution:
Parameter BSP can have a setting of Standard, Pedestal, Deadband or Deadband 0 %.
When you see the Keypad: BSP can be standard , Deadband, pedestal or pedestal at 0%.
The term is inverted on keypad.  Deadband should be Pedestal and pededstal /pedestal at 0% should Deadband/Deadband at 0%.
Same problem with SoMove:
The solution to set Pedestal like on ATV71, is to set Deadband on ATV6XX/ATV9XX.

Schneider Electric Egypt and North East Africa