{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
On the ATV630 and ATV930 process drives, why can't the digital input assignments be changed?
Issue:
ATV630/ATV930 the digital input assignments are not changing in the Input/Output menu?

Product Line:
Altivar Process, Altivar 630, ATV630, Altivar 930, ATV930

Environment:
All models

Cause:
Attempting to change DIx assignments in the COMPLETE SETTINGS > INPUT/OUTPUT menu

Resolution:
The digital input assignments in the INPUT/OUTPUT menu are read only.  To change an assignment, you need to go to the desired function and then assign an Input to the function. Example: to assign Reverse to DI2, you need to go to "Reverse assign" in the Command and Reference menu, and change that to DI2.

Link to the ATV600 programming manual:  https://download.schneider-electric.com/files?p_Doc_Ref=EAV64318
Link to the ATV900 programming manual;  https://www.se.com/us/en/download/document/NHA80757/

Schneider Electric Egypt and North East Africa