Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the maximum allowable temperature on the terminals of a Masterpact NW ACB?
Masterpact NW ACBs comply with IEC 60947-2. Temperature rise tests for Masterpact NW ACBs are specified in standard IEC 60947-2. Please find attached a declaration of conformity illustrating the maximum allowable temperature on the terminals of the Masterpact NW ACB.
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: