{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How is a Jog function set up on the ATV630 Drives?
Issue:
Setting up jog function similar to the other Altivar Drives

Product line:
Altivar 630, Altivar 650, Altivar 660

Environment:
all

Cause:
n/a

Resolution:
A Jog function is not available on the Altivar 600 series drives. It is available on the 900 series drive.

If the VFD is set for 3-wire control, then change to the 900 series.
If the VFD is set for 2-wire control, then the Preset Speeds function may be acceptable.  Note that the Preset speed used for the jog speed will not run the motor at less than the Low Speed setting.

Schneider Electric Egypt and North East Africa