Search FAQs
What is the part number for the Ethernet IP Module for the Altivar Process Drive?
Issue:
Part number for the Ethernet IP Module for the Process Drives
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)
Environment:
All serial numbers for Altivar Process Drive
Cause:
Part number required to order part
Resolution:
Altivar 600
Part Number - VW3A3720
Used for communication of Modbus TCP or Ethernet IP protocol on the Altivar Process Drive
Multi-Drive Link
Part Number - VW3A3721
Used for linking multiple Altivar 600 drives when using the Multi-Pump functions in addition to Modbus TCP or Ethernet IP.
Altivar 900
Ethernet IP is embedded on the drive so there is no option card module
Part number for the Ethernet IP Module for the Process Drives
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)
Environment:
All serial numbers for Altivar Process Drive
Cause:
Part number required to order part
Resolution:
Altivar 600
Part Number - VW3A3720
Used for communication of Modbus TCP or Ethernet IP protocol on the Altivar Process Drive
Multi-Drive Link
Part Number - VW3A3721
Used for linking multiple Altivar 600 drives when using the Multi-Pump functions in addition to Modbus TCP or Ethernet IP.
Altivar 900
Ethernet IP is embedded on the drive so there is no option card module
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: