{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is an Altivar ATV320 rated for variable or constant torque loads?
Issue:
Is ATV320 rated for variable or constant torques?

Product Line:
Altivar 320, ATV320 Machine Drive

Resolution:
The ATV320 is designed for both variable torque and constant torque loads.

In the Motor Control menu (drC-), there is a parameter Motor Control Type (Ctt) selection for the application.  Among others, the basic selection is:
Std (Standard) for a linear V/F ratio which is typical for constant torque loads
uF9 (V/F Quad) for a curved V/F ratio which is typical for variable torque loads

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)

Schneider Electric Egypt and North East Africa