{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can other manufacturer's cabinets be installed in the HyperPod?
Issue:
Does HyperPod support other cabinet manufacturer's, or just APC NetShelter?

Product Line:
HyperPod

Environment:
All versions and serial ranges

Cause:
Customers may want to install a 3rd party cabinet into the HyperPod.

Resolution:
Yes, 3rd party cabinets can be installed in the HyperPod easily. Height differences are no problem with the adjustable brush strips that mate with the cabinet roof.

Schneider Electric Egypt and North East Africa