Search FAQs
Is it possible to read Somachine PLC_R structure tag from the Magelis HMI?
Issue:
Is it possible to read SoMachine PLC_R struct from the Magelis HMI?
Product Line:
SoMachine v4.x, EcoStruxure Machine Expert
Environment:
Symbol Configuration in PLC Programming Software for Windows
Resolution:
In SoMachine and EcoStruxure Machine Expert, it is possible to read PLC_R directly from an HMI programmed with Vijeo Designer.
Steps:
1) Add the Symbol Configuration Node from the Tools tree to your PLC:
![Add Symbol Configuration node Add Symbol Configuration node](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000CcV9PQAV&oid=00DA0000000abSmMAI)
2) In the menu bar of the Symbol Configuration pane, activate "Unconfigured from Libraries"
![View -> Unconfigured from Libraries View -> Unconfigured from Libraries](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000CcV9QQAV&oid=00DA0000000abSmMAI)
3) Click Build.
![Build from Symbol Configuration pane Build from Symbol Configuration pane](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000CcV9RQAV&oid=00DA0000000abSmMAI)
4) From Symbol configuration, expand the SEC -> PLC_GVL -> PLC_R and place a tickmark next to PLC_R:
![Tick the checkbox next to PLC_R Tick the checkbox next to PLC_R](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000CcV9SQAV&oid=00DA0000000abSmMAI)
4) In Vijeo Designer, right-click on the Variables node and select "Import Variables From SoMachine..."
![Vijeo Designer Navigator - Import Variables From SoMachine.... Vijeo Designer Navigator - Import Variables From SoMachine....](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000CcV9TQAV&oid=00DA0000000abSmMAI)
5) In the "Import SoMachine Variables" dialog, expand the nodes and choose the specific variables you want to use in Vijeo Designer:
![Import SoMachine Variables Import SoMachine Variables](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000CcV9UQAV&oid=00DA0000000abSmMAI)
NOTE:
1) PLC_R.ilwSystemFault_1 and PLC_R.ilwSystemFault_2 variables will not be imported into Vijeo Designer because they are LONG WORDs (64-bit datatypes) - which are not supported by Vijeo Designer
2) Enumerated types that have Strings associated with them from the PLC will only appear as the Integer Value in Vijeo Designer. So you will have to look up the value's context from the manual when seen on the screen.
Is it possible to read SoMachine PLC_R struct from the Magelis HMI?
Product Line:
SoMachine v4.x, EcoStruxure Machine Expert
Environment:
Symbol Configuration in PLC Programming Software for Windows
Resolution:
In SoMachine and EcoStruxure Machine Expert, it is possible to read PLC_R directly from an HMI programmed with Vijeo Designer.
Steps:
1) Add the Symbol Configuration Node from the Tools tree to your PLC:
2) In the menu bar of the Symbol Configuration pane, activate "Unconfigured from Libraries"
3) Click Build.
4) From Symbol configuration, expand the SEC -> PLC_GVL -> PLC_R and place a tickmark next to PLC_R:
4) In Vijeo Designer, right-click on the Variables node and select "Import Variables From SoMachine..."
5) In the "Import SoMachine Variables" dialog, expand the nodes and choose the specific variables you want to use in Vijeo Designer:
NOTE:
1) PLC_R.ilwSystemFault_1 and PLC_R.ilwSystemFault_2 variables will not be imported into Vijeo Designer because they are LONG WORDs (64-bit datatypes) - which are not supported by Vijeo Designer
2) Enumerated types that have Strings associated with them from the PLC will only appear as the Integer Value in Vijeo Designer. So you will have to look up the value's context from the manual when seen on the screen.
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: