{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

Do we have an interlock for RM6 circuit breaker function that prevents remote operation (motor) while a manual operation is being performed?

In RM6 standard wiring for motorized circuit breaker function, the motor is being interrupted (i.e. not allowed to operate) via dedicated limit switches in case of operation of either the manual hand lever for circuit breaker, the manual hand lever for earthing switch or a locking action.
An example wiring diagram showing the limit switches as below.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: