Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
TeSys T Operating Modes and IO Logic
Issue:
What are the different TeSys T Operating modes? How are they different? 

Product Line:
TeSys T Motor Management Controller

Environment:
North American Products

Cause:
Installation and Application 


Resolution:
There are six main types of operating modes. Overload, independent, reverser, two-step, two-speed, and custom operating mode. Each has different wiring as well as specific behaviors for the TeSys T inputs and outputs. 
See attached for more information. 

Schneider Electric Egypt and North East Africa

Attachment(s)
Operating Modes (wiring and io logic).pdf [852.03 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: