{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video: How to upload and save the project file from the Twido PLC?

Article available in these languages: Japanese

Issue:
How to transfer a project file from the Twido PLC to the PC.

Product Line:
Twido Controllers and TwidoSuite Software.

Environment:
TwidoSuite

Resolution:
The Twido PLC powered on,
The communication cable TSXCUSB485 + TSXCRJMD25 (USB to RJ45 to RJ45 to minidin8) and the programming software TwidoSuite.

1) Run the TwidoSuite and choose "Programming" mode
2) From the "Project" tab, click "Open an existing project"
3) Check "From Controller",
4) Then click "Load".
5) The TwidoSuite will then jump to the "Select connection" page, choose your com port and click "OK".
6) Then the program existed in the controller will be transferred to the PC.
7) To save the project, you need to disconnect the PC from the PLC first. After this is done, the "Save current project" selection should be available from the "Project" tab.
8) Finally, select the location and file type to save your project.

NOTE: Twido is obsolete and the recommended replacement would be the Modicon M221 Nano PLC with EcoStruxure™ Machine Expert (formerly Somachine Basic) and can import the Twido program.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: