{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Does Ecodial comply with IEC 60363 OR IEC 61363 for marine applications design
Ecodial is best suited for Building Application and we do not recommend for Marine applications.
Ecodial follows the following IEC standards
  • IEC 60947 Standards for low-voltage switchgear and controlgear
  • IEC 60364 for installation standard mainly cable installation methods.
  • CENELEC TR50480 for Short circuit calculation.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.