Issue
Customer is looking for a new firmware upgrade
Product Line
PM5500 Series Meters
Environment
Firmware upgrade
Cause
Customer needs to upgrade PM5500 series meter upgrade
Resolution
RELEASE NOTES:
PM55xx firmware upgrade to address bug fixes, performance, and new features.
Updates:
New Features
DPWS feature: Allows self-discovery of the meter when connected in Local Area Network
• Added MAC Address within the display of the HMI.
Corrections
• Webpage new user password not stored at first time: Fixed
• Watch dog timer implemented to address communication loss
Additional fixes
This firmware update is intended for PowerLogic PM5560 / PM5563 Basic Power Meters.
Direct Firmware Links:
Please see attached below: PM5560_PM5563_V2.4.3.zip
How to upgrade PM55xx firmware:
Please see FA299853.
Customer is looking for a new firmware upgrade
Product Line
PM5500 Series Meters
Environment
Firmware upgrade
Cause
Customer needs to upgrade PM5500 series meter upgrade
Resolution
RELEASE NOTES:
PM55xx firmware upgrade to address bug fixes, performance, and new features.
Updates:
New Features
DPWS feature: Allows self-discovery of the meter when connected in Local Area Network
• Added MAC Address within the display of the HMI.
Corrections
• Webpage new user password not stored at first time: Fixed
• Watch dog timer implemented to address communication loss
Additional fixes
This firmware update is intended for PowerLogic PM5560 / PM5563 Basic Power Meters.
Direct Firmware Links:
Please see attached below: PM5560_PM5563_V2.4.3.zip
How to upgrade PM55xx firmware:
Please see FA299853.
Released for:Schneider Electric Egypt and North East Africa