Issue:
Specifications for the PTC Input on the VW3A3203 Option card.
Product Line:
ATV320 and ATV340 drive
Environment:
All
Cause:
PTC resistance input for the option card.
Resolution:
• PTC:
- 3 or 6 thermal sensors mounted in series (configurable by software)
- Thermal sensor current: 1mA maximum
- Nominal value: <1.5 kΩ
- Overheat trigger threshold: 3 kΩ
- Overheat reset threshold: 1.8 kΩ
- protected for low impedance: <50 Ω
- detection of high impedance: >100kΩ
Specifications for the PTC Input on the VW3A3203 Option card.
Product Line:
ATV320 and ATV340 drive
Environment:
All
Cause:
PTC resistance input for the option card.
Resolution:
• PTC:
- 3 or 6 thermal sensors mounted in series (configurable by software)
- Thermal sensor current: 1mA maximum
- Nominal value: <1.5 kΩ
- Overheat trigger threshold: 3 kΩ
- Overheat reset threshold: 1.8 kΩ
- protected for low impedance: <50 Ω
- detection of high impedance: >100kΩ
Released for:Schneider Electric Egypt and North East Africa