{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How to use ION Setup to determine how many modules are available for a given ION meter

Issue
Need to determine the number of a specific module either available or in use for a certain meter ION based meter.

Product
ION Supported meters including PM8000

Environment
ION Setup

Resolution

1) Connect to the meter with ION Setup (see ION Setup user guide here)
2) Place in Advanced configuration mode (see ION Setup user guide here) pg.72
3) Click on the folder to highlight to modules in question
4) Hover over the module and wait for tool tip to display the number of modules used and the number available.
Advanced Mode Configuration>> Data Rec Modules

The video below shows how to use ION Setup to determine how many modules of a certain type are available or in use for a given ION meter.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: