{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the PME databases have their compatibility level upgraded?
Issue
A customer is wanting to upgrade the compatibility level for their PME databases within SQL Management Studio and wants to know if this will cause issues.

Product Line
Power Monitoring Expert 8.x

Environment
SQL database Compatibility level

Cause
Customer would like to know if their PME databases compatibility level can be upgraded.

Resolution
With version 8.2, all PME databases are currently developed and tested using the "SQL Server 2008 (100)" compatibility level, as shown below.  Although newer versions of SQL server are supported with PME it is not recommended to upgrade beyond this.

Database Properties

Schneider Electric Egypt and North East Africa