Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the function of Masterpact Earthing switch and how to guarantee operator safety ?
The earthing switch is used to interconnect and earth the phase and neutral conductors of an electrical installation to ensure the safety of personnel during servicing.

To achieve this function,it is recommended to have locking in earthed position by 3 padlocks ,and this can be achieved when:
1-the Earthing Switch must be in "connected" position in a chassis equipped with an earthing kit
2-the Earthing Switch must be in “ON” position.

Under these conditions, the installation is earthed.

So,When the Earthing Switch is locked in earthed position:
1-it cannot be moved to "disconnected" position (a shutter prevents insertion
of the racking handle)
2-it cannot be turned "OFF" (a shutter prevents access to the "OFF" pushbutton). 

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more