Issue:
Motor control types information for the ATV320 drives
Product Line:
ATV320
Environment:
All
Cause:
Motor control types
Resolution:
The motor control type (Ctt) parameter is located in the DRC menu: DRI- > CONF > FULL > DRC
Details can be found on page 105 of the ATV320 Programming Manual NVE41295:
https://www.se.com/us/en/download/document/NVE41295/
Note: The Programming Manual lists some suggested application types for certain Motor Control Types. These are general suggestions. The Motor Control Type may need to be adjusted for your particular application.
For example: V/F Quad is listed for pump and fan applications. This means that V/F Quad generally works well with pump and fan applications, BUT it may not necessarily work well with your particular pump or fan. You'll need to
determine which Motor Control Type works best with YOUR motor.

Motor control types information for the ATV320 drives
Product Line:
ATV320
Environment:
All
Cause:
Motor control types
Resolution:
The motor control type (Ctt) parameter is located in the DRC menu: DRI- > CONF > FULL > DRC
Details can be found on page 105 of the ATV320 Programming Manual NVE41295:
https://www.se.com/us/en/download/document/NVE41295/
Note: The Programming Manual lists some suggested application types for certain Motor Control Types. These are general suggestions. The Motor Control Type may need to be adjusted for your particular application.
For example: V/F Quad is listed for pump and fan applications. This means that V/F Quad generally works well with pump and fan applications, BUT it may not necessarily work well with your particular pump or fan. You'll need to
determine which Motor Control Type works best with YOUR motor.
Released for:Schneider Electric Egypt and North East Africa