{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ATV32 ATV320: How do you assign a Freewheel Stop (rather than ramp stop) and a Run Permissive?
Issues:
When configuring an ATV32 or ATV320: How do you set the drive to always stop by Freewheel and assign a Run Permissive?

Product Line:
ATV32 ATV320

Environment:
ALL

Cause:
Input to Stop

Resolution:
On the keypad of the drive, you will press the dial and go to the following:
Freewheel Stop Always:  ConF > FULL > FUn- > Stt > Stt and set to nSt
Run permissive input:  ConF > FULL > FUn- > Stt > nSt and assign that to a Logic/Digital Input.
**Keep in mind that Freewheel Stop [nSt] is an active Low input, so if you do not have the wiring in place, the drive will be locked in nSt state.  Add a jumper from 24v to DIx/LIx assigned input until you have the actual contact installed.

Schneider Electric Egypt and North East Africa