Search FAQs
SFT2841 Setting and Operation Software Overview
Issue
Overview of the SFT2841 software for the SEPAM relay.
Product Line
SFT2841
SEPAM 20
SEPAM 40
SEPAM 80
Resolution
The SFT2841 software is the setting and operating tool for SEPAM series 20, SEPAM series 40 et SEPAM series 80. It may be used in 2 operating modes:
Overview of the SFT2841 software for the SEPAM relay.
Product Line
SFT2841
SEPAM 20
SEPAM 40
SEPAM 80
Resolution
The SFT2841 software is the setting and operating tool for SEPAM series 20, SEPAM series 40 et SEPAM series 80. It may be used in 2 operating modes:
- unconnected to SEPAM, to prepare parameter and protection settings
- connected to SEPAM, to download and upload SEPAM parameter and protection settings and have access to all operating functions.
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: