{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Power/Heat dissipation of SP334E?

SCADAPack 334E power consumption in the worst case is about 4.9W (4.5 + 0.3 + 0.020*24*2) with Analog outputs drawing full current.

Approximately 100% of the RTU's power consumption is converted into heat energy (a small amount will be converted into light energy rather than heat energy due to LEDs).

So the RTU outputs a little under 5 W of heat energy. This doesn't include the heat output of other devices or the external power supply that is providing power to the RTU.

Schneider Electric Egypt and North East Africa