{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: Using a braking resistor with Altivar Process ATV930 variable speed drive.
Issue:
Using a braking resistor with Altivar Process ATV930 variable seed drive.

Product Line:
Altivar Process ATV930 variable speed drive

Environment:
Where a braking resistor is needed

Cause:
Documentation

Resolution:
Use PA+ and PB power terminals of an Altivar900 series drives to connect a braking resistor

References with a "C" letter at the end: the drive does not have an internal braking transistor (chopper). Additional braking unit is required to connect a braking resistor

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.