{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can ATV320 be powered by DC bus using Bonitron unit?
Issue:
Can I use Bonitron unit connected on the DC bus to power up the ATV320 drive?

Product Line:
ATV320, Altivar 320

Environment:
All

Cause:
Customer has 1-phase line power.

Resolution:
Technically, if the Bonitron unit is sized properly, it could work. However, We have not tested that combination, and we have no UL listing on it.

Schneider Electric Egypt and North East Africa