This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Regarding the residual current devices ,are used mainly for human protection against direct and indirect contact,and they are defined by their sensitivity and interference immunity (type AC,A,SI and B).Please refer to catalog pages attached for the selection of the suitable type and some characteristics of these devices.