Search FAQs
VAMP 200 series Communication register lists
Product Line
VAMP 210/230/255/257/259/265
Resolution
Attached below are the Modbus, Profibus, Spa Bus, DNP3, IEC101, IEC 103 register lists for the following vamp series relays: 210/230/255/257259/265 respectively.
VAMP 210/230/255/257/259/265
Resolution
Attached below are the Modbus, Profibus, Spa Bus, DNP3, IEC101, IEC 103 register lists for the following vamp series relays: 210/230/255/257259/265 respectively.
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: