Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Video: How to Run a Manual Self-test on your Symmetra PX10-80KVA UPS

Article available in these languages: Spanish

Issue:
How to Run a Manual Self-test on your Symmetra PX10-80KVA UPS
 
Product line:
Symmetra PX1
 
Environment:
All Product models, all serial numbers
 
Cause:
At times it is necessary to perform a battery system test outside normally scheduled intervals
 
Resolution:
Select "Control" from the main Menu
Select "Do Self Test" and hit enter

Confirm the option by selecting Yes and hitting enter (The test will run for 1 minute)
 
You can monitor the status of the batteries while the test is running by Hitting Escape to get back to the main menu

Select "Status" from the main menu
Scroll down the list to Battery Voltage.

Make a note of the Actual Battery Voltage and How low it goes during the test. When the test is completed this number will start climbing. Value should be as close to 192v as possible. Lower values indicate the batteries are getting weak.

The following video demonstrates this procedure:
 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: