{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can legacy PWX , Concept or PL7 projects be converted to M580?
There are no means for taking the Legacy project straight to M580. There are no planned changes in this area.
  1. Conversion from Legacy to Unity Quantum/Premium is done with the embedded converter in Unity Pro
  2. Conversion from Unity Quantum/Premium to M580 is done with the Unity M580 Application Converter.
  3. If moving forward, it is necessary to convert from M580 w/QNTM IO to M580 with X80 IO that can also be done with UMAC.

Schneider Electric Egypt and North East Africa