Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Why, while configuring an IO module via the Dual Setting (Configure > Protection), does Ecoreach change the parameters for Inputs 5 and 6 of the IO module? (Configure > IO Config)
Issue:  While configuring an IO module via the Dual Setting (Configure > Protection) through Ecoreach the parameters inputs 5 and 6 of IO module are also changed.

Product Line: IO module, Ecoreach.

Cause:  Every time that user changes the configuration of an IO module and Control Unit, Ecoreach modifies the Inputs 5 and 6 of the IO module to ensure maximum coherence and security.

Resolution: ​After configuring the Dual Setting, check that the Inputs 5 and 6 of the IO module are configured properly. If not, configure them as required and click Write to Device.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more