undefined [object Object]
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can an option card be installed on an ATV320... C (compact) drive?

Issue:
ATV320...C (compact) drive option card installation.

Product Line:
Altivar 320 Compact

Environment:
All

Cause:
Option card

Resolution:
To install a communications or an option card in general on an ATV320 with C suffix, you must first have an option module adapter VW3A3600.
image1
https://www.se.com/ww/en/product/VW3A3600/mechanical-adapter-for-communication-module---for-atv320-compact-drive/

This applies to ATV320...C (compact versions) only.  The ATV320.. B (bookshelf version) has a slot cover on the bottom where it can accept one option card as standard.

Installation Instructions attached.

Schneider Electric Egypt and North East Africa

Attachment(s)
ATV320_IS_Option_module_adapter_NVE22661_01.pdf [570.79 KB]