{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PME 8.2 Vista crashes when trying to modify the scale on a horizontal or vertical bar views of a numeric object
Issue
In order to modify the scale on a numeric object with a  horizontal or vertical bar view in Vista, one must go to the Object Configuration and right click on the numbers in the preview.  In PME 8.2, there is an issue where this causes Vista to crash giving the following error message.



Product Line
Power Monitoring Expert 8.2

Cause
This has been logged as a bug in PME 8.2 and is being worked on for PME 9.0

Resolution
The workaround is to only right click the tick marks in between the numbers instead of the numbers themselves.  That way, it will work as previous PME versions and give you the ability to change the horizontal or vertical axis depending on which style was selected.

Schneider Electric Egypt and North East Africa