Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Can the WSOS V5 Software work on Windows 10?
Issue
Does WSOS V5 software support Windows 10?

Product Line
WSOS

Environment
Reclosers

Resolution
Version 5.16XX has support for Windows 7 and above, so it will work for Windows 10.

This is from page 6 of the release notes of the software

"Release version 5.16.xx of the Windows Switchgear Operating System allows the users to install and run the engineering tool on Microsoft Windows®10 operation system, which was not possible with the previous WSOS version 5.15.xx.

There is no change to the installation process. Double clicking on the installer and following the instructions on the installation wizard screen will guide the user as required.

The same version can be installed on Microsoft Windows 7 or Microsoft Windows 8 Operating systems as well."



 

Schneider Electric Egypt and North East Africa

Attachment(s)
WSOS5 - Release note-Version-03.pdf [998.04 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.