{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video: How to find Com'x IP address ?

Issue
Packets captured via Wireshark do not contain the Com'X IP address

Product Line
Com'X 200, Com'X 510

Environment
Wireshark, Com'X gateways

Cause
The Com'X does not transmit its IP address using ARP protocol upon power cycle like the EGX 100/300 gateways.

Resolution
If you are using Windows 7 or Windows Vista, the device should appear as a Network Device.
  • Disconnect your computer from all networks (all wired and/or wireless networks).
  • Connect an Ethernet cable between your PC (configured as  DHCP client) and the Ethernet 2 port on the Com'X.
  • Open Windows Explorer and click on Network, the Com'X appears in the list of devices.
  • Double-click the Com'X, the login page automatically opens in your browser.
  • Type the user name (admin by default) and password (admin by default).
  • Then click OK.
  • The IP can be found under Settings > General Settings > Network Settings.
Note: If accessing the meter for the first time, the factory set IP for both Ethernet ports is 10.25.1.1.

Details steps are shown in the below video.


Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: