Search FAQs
What are the main features of EM6400NG meter ?
The EM6400NG meter supports many features, a few of the features are listed
below:
• LED display screen: Intuitive self-guided navigation using three buttons LED
display, with three lines of concurrent values. Two columns of LEDs given on
the either side of the meter’s front panel indicate the parameter name being
displayed.
• Energy accounting and balancing
• EM6400NG POP (Class 1.0 and 0.5S) and RS - 485 (Class 1.0, 0.5S, and 0.2)
models
• THD% and individual harmonics up to 15th order for voltage and current.
• Active, reactive, and apparent energy readings
• Min/Max values of instantaneous parameters with timestamp.
• Cyber security: The meter enables disabling the RS - 485 port through front
panel keys against unauthorized access. This feature can also be used for
toggling between the RTU devices in case of limited availability of nodes in
software system.
• Measurement of both True PF and Displacement PF
below:
• LED display screen: Intuitive self-guided navigation using three buttons LED
display, with three lines of concurrent values. Two columns of LEDs given on
the either side of the meter’s front panel indicate the parameter name being
displayed.
• Energy accounting and balancing
• EM6400NG POP (Class 1.0 and 0.5S) and RS - 485 (Class 1.0, 0.5S, and 0.2)
models
• THD% and individual harmonics up to 15th order for voltage and current.
• Active, reactive, and apparent energy readings
• Min/Max values of instantaneous parameters with timestamp.
• Cyber security: The meter enables disabling the RS - 485 port through front
panel keys against unauthorized access. This feature can also be used for
toggling between the RTU devices in case of limited availability of nodes in
software system.
• Measurement of both True PF and Displacement PF
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: